Other Parts Discussed in Thread: HALCOGEN
Dear TI guys,
within HalCoGen (version 03.03.01) there can be set 8 PWM channels - AFAIK all 32 NHET pins/channels might be used for 32 different PWM signals. Is that right? Afterwards the tab "Pwm 0-7" can be perceived as non-complete but inspirational one, cannot? However, the amount of PWMs (=8) advises me that it was not chosen accidentally... ;-)
A period in this tab is editable and the shortest value which can be entered is 3.2us regardless defined value of VCLK2. It means maximal PWM frequency 312.5kHz. Of course, I am happy enough with this value. But theoretically I would expect e.g. 160MHz if VCLK2=160MHz, hr=1 and lr=1. OK, ithis extreme example is meaningless due to timeslots equal to one VCLK2 tick - one NHET instuction can be executed. However, why there is the limit of 3.2us?
Many thanks in advance,
Best regards
Jiri