This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

N2HET1[12] as output can't be set

Hello,

I've got a challange with the TMS570 NHET Io's.

Especially the N2HET1[12]. If I set this pin as output (DIR = 1) the DIN register bit is immediatelly 1 and output level is 3.3Volts.

I can not drive this pin to 0. I've already removed this pin from board so I do not have any contact to other sources.

If I use N2HET[16] with the same configuration this pin works correct.

Does anyone have an idea what is wrong and what the difference could be?

At IOMM N2HET1[12] is the default. It is now the second microcontroller where I do have this problem.

Thanks

Oliver