This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Explanation of Stellaris MCU's internal Temp Sensor formula...

So - the formula (immediately above) works easily & well enough - but from where did those key values originate?   Note: Data from LX4F datasheet.

For example: 147.5°C, 2.7V, 75 & 55.

One classical way to attack such a problem is to manipulate the formulas/givens to their limits.  Looking @ Vtens - it has negative, linear slope and is maximized when the right side term drives toward zero.  This occurs when TEMP = -55.  With TEMP @ -55°C, Vtens = 2.7V, its maximum.  Thus the 55 in our list of key values has been justified.  (55 "nulls out" the -55)

Now - how did this 2.7V originate?  It is a given - and results from the projection of the Volt/Temp "curve" into the X origin.  W/in the MCU die - this is likely a semi-conductor junction at/around a major dissipation point w/in the MCU.  The 2.7V value is a good 80%+ of Vdd and is sufficiently offset so that superb voltage regulation into the junction is provided.  Only temperature should impact this specially chosen MCU sense point.

Onto 147.5°C - how strange...  As our Volt/Temp curve is negative, and linear, this 147.5 results when the right side term of TEMP drives toward zero.  And this occurs when var ADCcode = 0.  Again - just as with the 2.7V - this is a given by the chip designer.  It's extremely doubtful that our die reaches this point -  the curve and internal configurations project this value. 

Only 75 remains - and it is the "slope" of the aforementioned Volt/Temp curve.  Its units are of interest - they are degrees/volt.   This is determined by dividing the "span" of the temperature (+147.5°C to -55°C = 202.5°C) by the "span" of the voltage (2.7V).   Thus 202.5°C/2.7V = 75°C/volt.   As a check 75C/V * 2.7V = 202.5C.  This 75°C/Volt holds over the 2 smaller temperature ranges graphed - as well. 

Keep in mind that the MCU's internal die temp is almost always considerably higher than the MCU's surroundings.  And - if driving/controlling power electronics - the temperature of those power devices is likely to be of higher importance...

This MCU temperature sensing is a valuable feature - hope that this explanation raises the understanding and utilization of this capability...