This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDX570LS31CNCD Layout

Can the TMDX570LS31CNCD be inserted in right-angled DIMM slot (are the components mounted on both side of the PCB)?

  • FAZL,

    Sorry for the very much delayed response. Yes there are components on both sides of the 'LS31CNCD so I think the answer is no. If it isn't right angle but still some angle other than vertical, i'm not sure.
    The 'LS31 CNCD's that I have have fairly 'short' components on the back side as long as you do not populate the JTAG header. But if you use the 'LS12 CNCD there is a fairly large inductor on the back side...

    -Anthony