This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCAN Busy Bit for IF1 and IF2 Interface are seprate bits or same bit for both the RAM IFx Registers?

Hello Support,

There is a BUSY Bit in IF1CMD as well as IF2CMD registers.

Are they separate hardware bits or same for both IF1CMD and IF2CMD registers?

Reason being, when IF1CMD Busy Bit is SET, do I expect to see IF2CMD BUSY Bit also SET or they are independent of each other?

Is it possible to write to IF2CMD Register when IF1CMD register BUSY Bit is already SET?

Thank you.

Regards

Pashan