This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Information TPS65381-Q1



Gentlemen

We're using microcontroller line RM48 Hercules on a project to safety applications. As recommended power supply we are using the chip TPS65381-Q1. But in none of the documentation available we consumption values ​​of current and voltage of some peripherals.
I would like if possible the gentlemen could point me some documentation or some values ​​of the peripherals listed below?

Graciously

Peripherals:

CAN

GPIO

SPI

WACHTDOG

EMIF

NHET

FPU

FLASH

ECC

SECDD

PLL

EFUSE

CLOCK COMPARE MODULE

CPU SELF-TEST

LBIST

ESM

MPU

CRC

DMA

PCR

RTI

  • Hello Pablos,

    RM48 datasheet includes current consumption under normal operating mode, PBIST usage and under CPU self test condition for typical frequency condition. Also for flash programming and erase conditions.
    However we do not break down the current consumption to the level of each peripheral or the system modules that you listed above.

    Best regards,
    TI Hercules Support