Other Parts Discussed in Thread: LM3S2739
Dear Sirs,
I am surprised that a wonderful family of M3 processor is going to be NRND.
But anyway I have to deal with it.
I am currently redesigning a board for a slightly different application, and even if 40-60% of the code will remain the same I believe this configures it as a "new design".
So I am looking into the M4 series, finding very few active parts at the moment.
The former design was build on a LM3S2739, and I am looking for an M4 replacement part.
The design must be in production within few months.
It's a different design so I don't mind pin compatibility, but the following features are mandatory:
- PWM for Motor control
- Analog input, possibly more than 10 bits and 4 channels available on the older part
- CAN controller
- Some additional timers to be used as additional PWM
- Possibly the Floating point unit, even if not strictly necessary.
What available part can you suggest in the M4 series?
Or what preview part you suggest to be switched to future production part (pin compatible)?
Thanks.