This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reg SYSTICK interrupt problem

Other Parts Discussed in Thread: SYSBIOS

Hi,

i like to generate simple systick interrupt . i have attached my code below ,using emulator i can able to see that systick current value decrements but interrupt not generating when ever it  reaches zero. Please give me suggestion .

#include "driverlib/interrupt.h"
#include "driverlib/gpio.h"
#include "driverlib/sysctl.h"
#include "driverlib/systick.h"
#include "inc/hw_ints.h"
#include "inc/lm4f212h5qd.h"
void tamil (void)
{
static int t =0;
t++;
GPIOPinWrite(GPIO_PORTG_BASE,GPIO_PIN_2,0xFF);
}
void main()
{
unsigned long i=0,value,value2;
SysCtlClockSet(SYSCTL_USE_PLL | SYSCTL_OSC_MAIN|SYSCTL_XTAL_16MHZ|SYSCTL_SYSDIV_2_5 );
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOG);

i=SysCtlClockGet();
GPIOPinTypeGPIOOutput(GPIO_PORTG_BASE, GPIO_PIN_2);
SysTickPeriodSet(1000);
SysTickEnable();
SysTickIntEnable();
//IntEnable(15);
//IntRegister(FAULT_SYSTICK,tamil);
SysTickIntRegister(tamil);
IntMasterEnable();

while(1)
{
//GPIOPinWrite(GPIO_PORTG_BASE,GPIO_PIN_2,0xFF);
//SysCtlDelay(2666667);
//GPIOPinWrite(GPIO_PORTG_BASE,GPIO_PIN_2,0x00);
//SysCtlDelay(2666667);
value = SysTickValueGet();

}
}

regards,

Tamil