Other Parts Discussed in Thread: TMS570LS3137
Hello Forum,
I am developing a CPU Card using the TMS570LS3137, in the schematics of the TMS570LS3x/RM5x Hercules Development Card there are 10K Pull Up on each MibSPIxNCSx (R55,R56,R57,R58,R59, R60,R81,...). The Label says VCC_3V3 (Pull Up) and the schematics symbol says GND to me. Anyhow these signals have a default pull state of "Pull Up".
So my questions:
+ Are these resistors Pull Up or Pull Down
+ Why do I need them? (I use the MibSPI1 and MibSPI3 including NCS[n] Pins to connect two TMS570 together by SPI)
regards,
Lorenz