Other Parts Discussed in Thread: TMS570LS0432
Hello Support,
In the spna106a.zip example for Cortex-R4 Initialization Code, there is a function called fmcBus2Check().
Can you please confirm whether I need to enable [SET] the following bits inside Cortex-R4 core :
C9_PMCR_Register_Content -- Bit 4 -- CPU Event Export -- Enable export of the events to the event bus for an external monitoring block
C1_Auxiliary_Control_Register -- Bit 25 -- ATCMPCEN -- ATCM parity or ECC check enable
C1_Auxiliary_Control_Register -- Bit 0 -- ATCMECEN -- ATCM external error enable
for fmcBus2Check() to PASS the test of SECDED within Flash Wrapper?
Do I need to SET all the above BITS or only a few of the above bits or NONE?
Or, is it a DON'T CARE for all the above bits for fmcBus2Check() to PASS the test?
Please let me know which of the above case is valid.
Thank you.
Regards
Pashan