Other Parts Discussed in Thread: TMS570LS0432
Out of box, I am unable to get nowFlash to program the TMS570LS04 HDK dev board. I verfied the 16MHz clock verified on OSCIN pin. The dev board seems to have a tiny bit of test code in it, as the LEDs around the TMS570 blink a few times after a RESET, so really not sure why nowFlash is not happy.
I attach the debug output below... (My PC is running XP)
nowFlash version 3.42 Build (OFFICIAL)
Config file C:\ti\nowFlash\v3.42.01\nowFlash.cfg Revision: 1
Accessing device 0 through port 0x000
User specified emulator type TIXDS100V2.
Using board configuration file C:\ti\nowFlash\v3.42.01\brddat\board_tixds100v2_v
3_cortex_rxx.dat
Port driver "C:\ti\nowFlash\v3.42.01\drivers\tixds510cortexR.dvr" ... LOADED
Port address 0x000 target..initialize..connect..reset..halt..complete
Device ID value read=0x8048AD05 on port 0x000
Device is Hercules type with ECC, Unique ID=0x8048AD05, Minor Revision 0.
Device Identification=TMS570LS0432.0
Engineering Row ID=00000000
Lot Number =0
Flow Check =0x0000
Wafer Number=0
Die Location: X=0, Y=0
Target Frequency 80.00 MHz
Configuration file: v3.42 , file rev: 1
Algorithm library: F021_R4_BE.x70, Version 1.51
Writing 0x20046300 to DUT address 0xFFFFFF70 to configure PLL1
Writing 0x3FC0763D to DUT address 0xFFFFFF74 to configure PLL2
Error 182 - Measured frequency 0.00 MHz not within +/-30% of target 80.00 MHz
Please use '-pllcfg 0x<addr> 0x<value>' to adjust the PLL configuration