Hello,
1) The TRM (SPNU99a) mentions two ADC offset calibration methods. One method uses two points around the mid-point, the other uses those two plus the end-points. What are the advantages / disadvantages of both methods?
2) There is no mention of gain calibration. Is there a reason that gain calibration is not required, or would accuracy be improved by adding a manual gain cal?
3) Section 19.8.1 of the TRM says "This calibration sequence includes the conversion of an embedded calibration reference voltage followed by the calculation of an offset error correction value." Is this embedded calibration reference different from the externally supplied VREFHI?
Thanks, Charlie Johnston