Hello TI
I am using M4 to receive a 32-bit data stream through SSI. The Fss from Master will keep low when 32-bit transferring. I have 2 questions since I got all 0 which is not correct:
1. When SSI is in slave mode, the baudrate is determined by Master, so setting it has no meaning. But the setting function both in ROM and Flash version ask me to set baudrate, it is not logical. How to fill in the parameter of baudrate in this case? just a dummy number?
2. When does the interrupt occure during above reception? I set the SSI frame as 'Freescale SPI Frame Format with SPO=1 and SPH=1', the data width is16 bit.
Looking forward to your reply and thanks in advance.
Jackie from TRULY Semiconductors, China.