This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cleaning up linker cmd file for LM4F development with CCS and TI v4.9.5 toolchain

I am cleaning up the .cmd file for several projects.  Most of the .cmd file was auto-generated by CCS at project creation.  In the project's properties inside of CCS, I set my stack size to 2048.

I see some comments and linker commands that seem to be in conflict.  The comments are:

/* The following command line options are set as part of the CCS project.    */
/* If you are building using the command line, or for some reason want to    */
/* define them here, you can uncomment and modify these lines as needed.     */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone.              */
/*                                                                           */
/* --heap_size=0                                                             */
/* --stack_size=256                                                          */
/* --library=rtsv7M4_T_le_eabi.lib                                           */

But the last line of the file is not commented out and reads:

__STACK_TOP = __stack + 256;

It seems this last line is in conflict with what I set to 2048 inside of CCS.  Should this last line be removed, as I defined the stack ast 2048 in CCS?  It seems like the CCS property definition wins the day.