This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

URGENT: TMS570 Dual Core



Hi,

Is there a possibility of turning off one of the cores in the TMS570? The current draw while idling, non-sleep, ~390mA for both (or one, not sure) cores is a bit high.

Take care,

Charles

  • Charles,

    The two cores are running in lock step. It is not possible to turn one off.

    Thanks and regards,

    Zhaohong

  • As a further comment to Zhaohong's response, the additional CPU in lockstep is not a primary draw of leakage current on the product when the sum of all digital logic is considered.  Even if the option were present, disabling the checker CPU would not make a large difference in worst case device power consumption.  Consider utilizing the hardware power domains to disable unused regions of peripheral logic if static power reduction is needed.

    Regards,

    Karl