This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HET IDE problem

Hi experts:

    My HET IDE encounter a problem when I start it.

    "HET IDE could not parse \resource\hpetdevice definitions.xml file", the message suggest me reinstall the software, but the error comes again after re-installation.

    What's wrong?

   Thanks!!!

 

 

 

 

 

  • Hi, 

    Is this the actual quote?    Checking my installation of HET IDE I have a file 'resources\HETDeviceDefinitions.xml' but no 'hpetdevice_definitions.xml'.

    Some other things that would help to know:

     - version of HET IDE you are using.

      - OS version

      - OS language (English, or other character set?)

      - How was the HET IDE installed  (all users, just for you, or by another user on the same machine?)

    Also, if you look at the path to HET.EXE by clicking the properties of the icon in the start menu,

    and if you navigate to that folder  (for me that folder is:   C:\Users\a0xxxxxx\AppData\Local\Texas Instruments\Hercules\HET)

    do you see a resources subdir and which XML files are in that folder.


    Best Regards,

    Anthony

  • Hi Anthony:

        The actual information listed below:

    -OS Version: Windows XP

    -Language: English

    Thanks!

  • Hi Zhou1,

        Would you please check the version of you HET IDE?

    Is this your first time to run this software or you had run it for a long time and the error just showed up this time?

    Thanks,

        Ken

  • Hi ken Wang1:

       Thanks for your attention.

       This is my first time to run HET IDE.

        I never use this software before. Thanks!

     

     

     

     

  • Hi,

      would you please do me a favor to check the version of your HET IDE. and there are two ways you can do to try to fix the error. The first one is you can re-install the software with another path and check whether it works. the second one is you can send us the HETDeviceDefinition.xml file as the attached file in this post and we will check whether there is any syntax error of it.

    Thanks and Best Regards,

    Ken

  • Hi Ken Wang1

      The HET IDE software I have installed from " DRV8301-LS12-KIT".

      I have download the new soft HET IDE named "spnc016.zip", and it is running well.

      Thank you very much!!!

     

     

     

     

     

  • Hi  Zhou1,

         I'm so glad to hear that. Thank you for your support  of our forum.

    Thanks and Best regards,

    Ken