Other Parts Discussed in Thread: TLV803
I've got a very low power application (hibernates most of the time) currently served by a 8 bit MCU and I would like to migrate to a more flexible 32 bit ARM based MCU. The Stellaris Launchpad ((EK-LM4F120XL) seems to be a great way to try out the Cortex M MCUs from TI.
I realize I can prototype the application in the lab and measure application current by removing the V3,3/MCU_PWR (H24 - H25) jumper and bridging with an ammeter, but it's not clear if I can configure the LaunchPad board to run under low power. I really would like to use the Launchpad to demonstrate the Stellaris MCU working in the real application and not just in the lab.
I though it would be sufficient to disconnect the H24-H25 jumper and supply 3.3V via the boosterpack pin but that doesn't work for some reason. If I supply 5V via the boosterpack pin and keep H24-H25 connected it does work. *BUT* the green power LED (D4) is on... obviously it is not going to be very low power with that on.
So can the Launchpad board be configured to consume just a few µA while the MCU is hibernating?
Thanks,
Joe.