Hello,
I would like to have some informations about the Stellaris® LM4F120 LaunchPad. Basically I have an application where I would like to use a microcontroler based solution to send pulses (0-5V) to trigger 6 LED and 1 camera based on an external trigger that is asynchronous, but nearly periodical. The LED signals would have to be sent every 8 rising edges of the input clock, and this sequentially on each output ports while the camera signals will be sent every rising edges of the clock. I would like the possibility to have pulse width modulated signals and would like to output the different pulses on different physical ports (see drawing attached) that will be wired to the different LED (digital output 2 to 8) and camera (digital output 1). The frequency of the clock is between 3 Hz and 20 Hz. I would like to have the possibility to chose pulses with ON duration ranging from 10 us to several ms. I wanted to know if that was possible with the Stellaris® LM4F120 LaunchPad? If not what other TI solution should be prefered?
Thanks in advance,
Grégory