Hello,
I see that the EK-LM4F120XL examples (release 9453) don't include the bootloader examples (boot_serial, boot_demo1, boot_demo2). Can I use the ones included in the EK-LM4F232 release? The boot loader contains a non-trivial amount of assembly that I'd rather not have to recode. If those examples won't work then which ones will work on the EK-LM4F120XL?
Thanks,
Derek