Other Parts Discussed in Thread: LM3S3748
We recently upgrade from an LM3S3748 to the LM3s5B91 for increase in flash capacity and pin compatibility. We have just become aware of the NRND status. In reading posts on this subject it is the impact on distribution stock that concerns me due to this status. We are just beginning production and having to redesign already is time-consuming and costly. The other issue is that the M4 parts currently available do not support the memory configuration of the previous parts. This will mean I have to move to another manufacture to maintain specification of design.
The parametrics on the M4 so far shows a maximum ram size of 32K. The 3748 was 64K and the 5B91 was 96k. Will there be parts with higher ram capacity in this familt and when?