This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EMIF signals control

Hi,

according to spnu499a, 4.3.3:

Control for other EMIF Signals:

Bit 31 of the system module control register GPREG1 at address 0xFFFFFFA0 is used to gate off the EMIF module outputs: EMIF_ADDR[0], EMIF_ADDR[1], EMIF_ADDR[6], EMIF_ADDR[7], EMIF_ADDR[8], EMIF_BA[1], EMIF_nCS[0], EMIF_nCS[3]. These 8 signals are multiplexed with NHET2 signals. By default, these terminals are tri-stated and pulled down. Any application that requires the EMIF functionality must set GPREG1[31]. This allows these 8 EMIF module outputs to be driven on to the assigned balls. 


But I don't see any mention of bit 31 in GPREG1 (2.5.1.34).

Which one is correct ?

Tristan.

  • Hi Tristian,

    We are looking into this and will get back to you shortly.

     

    Hercules forum support

  • Hi Tristan,

         The above clarification is correct. You should enable these EMIF terminals by setting the GPREG1[31]( system general-purpose register).Please refer to the previous post for this issue:

           http://e2e.ti.com/support/microcontrollers/hercules/f/312/p/202026/717735.aspx#717735

          Hope that this may help you.Thanks.

    Best Regards,
    Shelford

  • and below statement is true:

     Tristian,

    The statement below is true

    • Control for other EMIF Signals:

    Bit 31 of the system module control register GPREG1 at address 0xFFFFFFA0 is used to gate off the EMIF module outputs: EMIF_ADDR[0], EMIF_ADDR[1], EMIF_ADDR[6], EMIF_ADDR[7], EMIF_ADDR[8], EMIF_BA[1], EMIF_nCS[0], EMIF_nCS[3]. These 8 signals are multiplexed with NHET2 signals. By default, these terminals are tri-stated and pulled down. Any application that requires the EMIF functionality must set GPREG1[31]. This allows these 8 EMIF module outputs to be driven on to the assigned balls.

     

    We will look it why bit 31  is not relected in the GPREG1 definition.

     

    -Hecules forum support

     

  • Hi,

    thank you for the reply.  However, even with that change, I still cannot use the SDRAM on the HDK.  Do you have any sample code for it ?

    Tristan.