Other Parts Discussed in Thread: TMS570LS3137
Hi everyone,
I need some help. I'm trying to use SPI port as GIO, but I can't write in the registers
Environment:
Target: TMS570LS3137
IDE: IAR worckbench
#define STD_OFF 0
#define GPIO__OUTPUT 1
#define GPIO__MBSPI1_addr ((gioPort_t *) 0xFFF7F418U)
#define GPIO__MBSPI3_addr ((gioPort_t *) 0xFFF7F818U)
#define GPIO__MBSPI5_addr ((gioPort_t *) 0xFFF7FC18U)
/* Set MBSPI5 CS[0] as output */
GPIO__MBSPI5_addr->DOUT |= (STD_OFF<< 0);
GPIO__MBSPI5_addr->DIR |= (GPIO__OUTPUT<< 0);
/* Set MBSPI1 SIMO[0] as output */
GPIO__MBSPI1_addr->DOUT |= (STD_OFF<< 10);
GPIO__MBSPI1_addr->DIR |= (GPIO__OUTPUT<< 10);
But DIR register has no change. Always has the value of Zero (GPIO__MBSPIx_addr->DIR = 0). And therefore I can't use as digital output
Is there some register than prevents writing?
Thanks