Hi!
I having some issues with ICDI drivers in my Windows 7 PC (CCS Version: 5.2.1.00018). Really coundnt figure out what is going on. =(
Following the "Quickstart-Driver-Installation.pdf" document, in theory I should follow the steps below:
1) Go to Device Manager, I should see three "In-circuit Debug Interface" devices inside "Other devices" (with the yellow exclamation icon)
2) Right click on it e select "Update Driver Software"
3) Select the driver folder and install it.
4) After installed, "scan for new devices"
5) Repeat the installations steps for the remaining devices.
My problem is that after step 4 all devices completely disappeared in Device Manager. When I unplug/plug the board Windows doesnt take any action (doesnt recognize the device, like I am not even plugin the board in).
Every time I try to debug via CCS I get the following message: "Error connecting to the target".
LM programmer is also not working.
I already tried to:
- Uninstall CCS, delete C;/ti folder, reinstall CCS with admin privileges.
- Uninstall drivers manually and reinstall in Device Manager. I am actually able to install the drivers manually but all devices are showing the yellow exclamation point. Seeing the properties of the devices I get the message "This device cannot start. (Code 10)" in the device status box.
- Change COM ports
- Restart PC several times
- Tested with a different stellaris launchpad board (I have two boards).
- Update my Windows 7.
I hope you guys can help me with these issues!! =)
Thanks in advance!
Agk