This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Stellaris launchpad clock output

Hi!

I'm trying to use my Stellaris launchpad with a camera module (OV7670). First of all I need to supply a clock for the camera, and its frequency must be between 8 and 40 MHz. 

Can I supply the clock from the launchpad or I need to build a clock generator circuit?

Sorry for my bad english :)

Thanks!

  • Unstated is any requirement for this "clock" signal to be synchronized to any other signal/bus/event.

    That said - use of any of the MCU Timers - configured for PWM Mode - enables easy and direct output from that timer's external pin.  Further - you can control both the frequency as well as the duty cycle of the output.  I believe that you can output up to 1/2 of the MCU's System Clock - via this method.

    MCU Datasheet will reveal which pins are timers - and provide reasonable set-up & config detail.   In addition "SW-DRL-UG" will list & detail various functions available to achieve your objective.

  • Hi!

    Yes, I have tried this PWM method, but the result wasn't a square wave. I think I will build a circuit for that. Thanks!

  • G��bor K��rmendy said:
    but the result wasn't a square wave

    But it must be!  (and always has been such for our group.)

    Post your code - likely a failed SysCtlPeriphEn() which prevented a legitimate output. 

    Simply too easy for you to give up - expend needless effort - and produce something w/out the precision & flexibility of this powerful ARM feature...

  • Hi!

    I did not give it up, but I thought the gpio port can't follow that 10-14 MHz frequency. Meanwhile I discovered that the cabel I used with the oscilloscope have too much capacitance. Because of that I can't see the square waves. 

    Thanks for helping.

  • Glad that you persisted - got it. 

    Always best to KISS - start at relatively low frequencies - confirm the basics - then gradually increase.