Other Parts Discussed in Thread: TMS570LS3137
Hi,
For a project I need to connect many memory devices to the same TMS570LS3137, they are all similar and can work with the settings of a single nCS.
As far as I can see there is no reason why I cannot use a simple GIO to control the CE of all the memory ICs, the only draw back would be in that the code will run slower and hence a slower data throughput.
Have I over looked anything or is there something in the working of the TMS570 which will cause this idea not to work.
Cheers,
Alan