This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Crystal frequency on development kits?

Hi!

Can't find any information about the on-board crystal on the TMDX570LS31HDK and TMDX470MF066HDK development boards?

Thank you!

  • Andreas,

    I was not able to find any information on the crystal in the user's guide either (guessing that is where you checked). I am going to move this post over to the Hercules forum where they can get this information to you.

    Thanks,

    John

  • Hi Andreas,

    Both, the TMDX570LS31HDK and the TMDX470MF066HDK use a 16MHz on-board crystal.

    Manufacturer part number: 7A-16.000MAAJ-T; TXC CORPORATION (VA)

    Digikey part number: 887-1086-1-ND

    The valid oscillator frequency range is from 5MHz to 20MHz.

    Regards, Sunil