It would appear that an example application demonstrating the use of Composite Device Classes should exist for the LM4F232 (usb_dev_cserial), but this application is included in the examples supplied with StellarisWare for the LM4F232H5QD.
Does such an example exist? If so, where might I find it?
Note: I'm in the beginning stages to working my way through the USB interface, so it is possible that this example (and the Composite device Class) is not the approach I need to pursue, but I'm hopeful that by studying this example in concert with other resources I can reduce my learning curve a bit.
Thank you,
Kevin Taberski