Other Parts Discussed in Thread: TMS570LS20216
Hi there,
I configured DMA channel 15 to accept request from line #13 for RTI event1 that is happening every 60 seconds, using DMA Port B to perform transfer data from the on-MCU Flash ROM to the CRC module for 64-bit CRC check, for a total of 2 MB ROM - 1024 bytes.
The DMA module is configured with DMA parity check enabled.
Every 60 seconds when the CRC calculation request is made from RTI event1, ESM reported a DMA Parity Error (code 0x04). The 64-bit CRC was nonetheless computed.
Any hint as on where to look at?
Regards.