Other Parts Discussed in Thread: RM48L952, HALCOGEN
Hello,
I'm using Halocogen 4.03.00 for Rm48L952.
Is it possible to remap the interrupts inside of Halcogen (say, setting ADC1Group1 interrupt on channel 2 instead of channel 15)?
I did not find any edit possibilities, therefore I think is is not (yet) possible, correct?
So if I want to assign different priorities to the IRQ interrupts, I will have to do this in my code (setting the CHANMAP[x])?
And if I do this in code, I will lose the connection to halcogen (isr function names/position in vector, enable IRQ/FIQ setting, or at least a misleading label (saying "RTI compare 0" and I have to know that this is ADC1Group1))...
Perhaps I'm completely wrong, so before continuing to search for a workaround, I wanted to see if I missed the feature.
Thank you very much,
Best Regards,
Roger