Hi,
I am using a Hercules Dev Board with the RM46L852ZWT.
When I attempt to debug a program on this board in CCS 5.3.0, it gives me the following error now: "Texas Instruments XDS100v2 USB Emulator/CortexR4 : Target must be connected before loading program."
-My board is connected via the mini-USB and is powered.
-I have been debugging programs for the last week just fine, but all of the sudden it is telling me this now.
Any help would be appreciated. Also, I can get more information if this is not enough!