This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4F232H5QD: differential ADC problem

Hi,

I've just started development on LM4F232H5QD eval kit. My application need to use ADC in single ended mode and differential mode also.

Therefore I configured one channel (AIN3) to use in single ended mode with ADC0 module and other channels (AIN4 and AIN5) to form one differential pair (CH2) with ADC1 module.

Now my single ended channel is working flawlessly but differential pair is giving me some strange problem. Here is description of problem:

To make this differential pair working, I have to first configure these two analog channel as single ended analog input channel and measure some values and then configure (AIN4 and AIN5) in differential mode and measure voltage. But this measurement will work only till system reset. Once I restart controller, it will not work and stuck up. I have verified in Errata but nothing has been mentioned about it.

Since it is very early in development so I'm only polling the flag. For reference I'm also attaching the code.

If anyone can suggest something, it will be helpful.

3771.ADC_Init.c

Thanks,

Shriram

  • Hi Shriram,

     

        Please check the revision of the LM4F232 that you are using, and then take a look at the errata for the ADC: http://www.ti.com/lit/er/spmz636d/spmz636d.pdf

        The Revision is on the microcontroller part markings, third row, last two digits.  I have an LM4F232 eval board with the Rev. A1 part, so the ADC errata would affect my board.  You probably have Rev. A0 or Rev. A1 of the LM4F232. 

       

        Best,

          Rick Nardone 

      

  • Hi Rick,

    Appreciate your help.

    I've checked Rev No of LM4F232H5QD placed on my board. Its 'A1'. Therefore after referring to the errata, I noticed that additional settings needs to be done for proper functioning of external reference voltage (Section 11.1 'External reference requires additional configuration'). I have configured this setting but it didn't solve problem.

    I added one line in code to set the PB6 BIT as 'HWREG(GPIO_PORTB_BASE + GPIO_O_AMSEL) |= GPIO_PIN_6;'

    Regards,

    Shriram

  • HI Shriram,

    Check to see if you have the StepConfigure correct.  I think you need to ad the ADC_CTL_END to tell the sequencer you are at the end of the sequence.

    Your code:

    ADCSequenceStepConfigure(ADC1_BASE, SQNC_NUM_0, 0, ADC_CTL_D | ADC_CTL_CH2);

     

    Thanks,

        Rick

  • Good Morning Rick,

    Thanks for suggestion but I have tried this combination and  problem still persist.

    However, I was able to make it functional in differential mode in another fashion. Now I've reconfigured differential ADC using following settings - 

    1. 1msec Timer A used for triggering ADC (earlier, it was processor based trigger)

    2. Wrote ADC1_Sequence0_ISR in which cleared ADC interrupt, and read ADC data (earlier it was polling for raw interrupt status).

    Now my Initialization sequence of ADC looks like this:

    {

        SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1);
        while(!SysCtlPeripheralReady(SYSCTL_PERIPH_ADC1)){;}

        ADCSequenceConfigure(ADC1_BASE, SQNC_NUM_0, ADC_TRIGGER_TIMER, 0);
        ADCSequenceStepConfigure(ADC1_BASE, SQNC_NUM_0, 0, ADC_CTL_IE | ADC_CTL_END | ADC_CTL_D | ADC_CTL_CH0);
        ADCReferenceSet(ADC1_BASE, ADC_REF_EXT_3V); //errata
        HWREG(GPIO_PORTB_BASE + GPIO_O_AMSEL) |= GPIO_PIN_6;
        ADCSequenceEnable(ADC1_BASE, SQNC_NUM_0);
        ADCIntRegister(ADC1_BASE, SQNC_NUM_0, ISR_ADC1_Seqnc0);
        ADCIntEnable(ADC1_BASE, SQNC_NUM_0);
        TimerControlTrigger(TIMER0_BASE, TIMER_A, true);

    } //end of ADC init

    ISR looks like:

    {

        ADCIntClear(ADC1_BASE, SQNC_NUM_0);
        GPIO_PORTG_DATA_R ^= GPIO_PIN_2;
        slSampleCopied = ADCSequenceDataGet(ADC1_BASE, SQNC_NUM_0, &ulADC1_Count);

    } //end of ISR

    Now ADC is working in differential mode but concern still remains, why with processor based trigger and polling mechanism, it is not working.

    Now you have both kind of codes, would you be able to conclude ?


    Regards,

    Shriram

  • Hi Shriram,

     

    There is an exellent example of using the ADC in polled mode in the Stellaris Lanchpad Workshop: http://processors.wiki.ti.com/index.php/Getting_Started_with_the_Stellaris_EK-LM4F120XL_LaunchPad_Workshop?DCMP=Stellaris&HQS=StellarisLaunchPadWorkshop

    Take a look at the way this example clears the interrupt in polled mode. 

    Best,

        Rick