This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Setup 2 wire SPI on TMS570LS3137



Hi Guys,

I'm hoping to interface the FM24CL64B with the MiBSPI3 peripheral, is it possible to connect the SOMI and SIMO pins together and use them as a 2 wire SPI connection.

From the datasheet the receiver will acknowledge the receipt of data by pulling "SDA" to ground, this occurs for both the sending and receiving of data; can this be coded into the TMS570?  The only other condition is that the clock must be continuous.

Cheers,

Alan