Hi!
What are the access times to memories of the RM48L95ZWTT?
Regards,
Pierre.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
What are the access times to memories of the RM48L95ZWTT?
Regards,
Pierre.
Pierre,
A LDR or STR instruction onchip RAM takes 3 CPU cycles to complete.
Thanks and regards,
Zhaohong
Hello Zhaohong,
Is that 3 Cycle access time for On-Chip RAM is also true for TMS570LS0432 device?
Thank you.
Regards
Pashan
Pashan,
It is true for all TI devices based on Cortex R4. Cortex R4 tries to improve the accessing time by speculative fetch. If the data is already fetched into CPU buffer when LDR executes, it becomes a one cycle instruction.
Thanks and regards,
Zhaohong
Hello Zhahong,
In the following link :
http://www.arm.com/files/pdf/Cortex-R4-white-paper.pdf
I see that typical value is 2 cycles instead of 3 cycles as mentioned by you. Please confirm if ARM document is wrong.
I am assuming ATCM [Flash] and BTCM [RAM], both have 3 Cycles of Access Time as mentioned by you.
Thank you.
Regards
Pashan
Maybe "typical access time" = "average"... and average(3cyles normal mode,1cycle when fetched)=2cycles ?
It's so marketing!