This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4F SSI clock rate not what expected



Hi,

I'm using an LX4F230H5QR FIGA3 running at 50 MHz. Here is my clock init:

ROM_SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ | SYSCTL_OSC_MAIN);

The device is configured as an SPI master and it is my understanding that bit rates are achievable up to SysClk/2, which in my case is 25 MHz.

I'm trying to configure the bit rate to be as close to 16 MHz as possible. When I use this line to configure the SSI Clock:

SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_3, SSI_MODE_MASTER, 1000000, 16);

I always measure a few MHz faster bit rate on my oscilloscope than configured. And anything higher than about 12.8 MHz will just set the bit rate to 25 MHz.

I also tried direct register control to manually configure the ssi clock without the library using these lines:

HWREG(SSI0_BASE + SSI_O_CPSR) = 3;
temp = HWREG(SSI0_BASE + SSI_O_CR0);
HWREG(SSI0_BASE + SSI_O_CR0) = (temp & 0xFFFF00FF);

Setting CPSR to 3 and SCR to 0 should give me an ssi bit rate of about 16,666,666 Hz, but the bit rate actually ends up being 25 MHz.

Configuring the ssi clock to be low (around 1 or 2 MHz) will yield the proper rate, but as 13 MHz is approached, the error gets higher until the ssi module just uses 25 MHz.

I have verified that my system clock is running at 50 MHz as well.

I checked the errata for the part and found nothing relevant. Am I doing something obviously wrong here or is it just not possible?