Other Parts Discussed in Thread: HALCOGEN, TMS570LS3137
Sirs:
I am working with the Olimex TMS570-CAN board, trying to control LED1 and LED2. Schema for TMS570-CAN (TMS570LS20216SPGE ) indicates LED1=DMMDATA[11]/MIBSPI5SIMO[3] and LED2=DMMDATA[13]/mIBSPI5SIMO[1]. SPNS141F–JULY 2011, table 2-8 page 25 indicates pins are multiplexed. There is no multiplexing registers in the LS20216 part. Same document, section 4.6.2 page 49 indicates multiplexing is accomplished by enabling/disabling the MIBSPIP5 and DMM modules. I believe after deciding which module has pin control, you can then, in the module set-up, configure pins for either peripheral or GIO function to drive the LEDs. Are my assumptions correct?
When using HalCoGen V3.04.00 configured for TMS570LS20216SPGE (TMS570-CAN board processor): on the “General” tab the DMM Module is “Grayed” out, can I assume HalCoGen software is incomplete? Will I need to create my own DMM control routine? Do you have a solution to configure the TMS570-CAN board to drive LED1 and LED2?
Thank You, Leonard Cronk 08MAR13