This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Stellaris Launchpad: How to set a higher baud rate on the USB- serial interface



Is there any way to set the communication baud rate though the USB-serial interface to a higher value than the supported? I am using Win 7.

I know that I can set the Stellaris microcontroller baud rate to much higher (like 5Mbps). Since the distance between the the interface chip and the microcontroller is short, I think some higher baud rate would work as well. However, the standard driver on win 7 only accept baudrate max to 128kbps. I am wondering if there is anything I can change to overclock it.