This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tms570 halcogen freertos

Other Parts Discussed in Thread: HALCOGEN

Hello,

I created a freertosblinky application as the demo says in halcogen, but the program get in the dataentry intvect.

I`m working with the halcogen v3.0

In the past I worked with the halcogen v2.8 which has mixed the boxes in my screen. But the same demo configuration worked fine and led blinked.

 

Do you know any trouble in the halcogen or some other generation fail should lead to wrong demo.

Because when I select the TMDX570LS20SMDK then I can set the RTI options, when I select TMDX570LS216SZWT_FREERTOS then I cant see the tab.

 

I`m use the Kil TMDX570LS20SMDK  which has the TMDX570LS216SZWT cpu.

 

What is the difference betwee the two option? And what should I correct to clean the interrupts?