This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

nERROR pin and ESM Low-Time Counter Preload Register



I have tried to write to the ESM Low-Time Counter Preload Register ESMLTCPR while in supervisor mode but the register does not seem to change! Both ESMLTCR and ESMLTCPR have the value 0x3FFF. I would expect this of ESMLTCR but the manual states that ESMLTCPR should have the value 0x1 at reset. Can you tell me how I can write to ESMLTCPR in order to set the value of ESMLTCR. 

I require the nERROR pin to be set low for a very short time during eFuse, OTP 2bit ECC and RAM &FLASH 2bit ECC error checking as defined in your manual and initialisation example SPNA106C. After the self tests I then want to configure the nERROR pin to be low for a longer time. In this way my external circuitry can distinguish between internal startup tests and actual errors based on the length of the nERROR pin pulse.