Hi,
I am trying to use the CAN peripheral with this board. I understand that we need to connect an external CAN transceiver for CAN communication to work. I tried using the MCP2551 from Microchip and the simple_tx.c example code provided by TI. I changed the CAN pin definitions given in the simple_tx.c program to ones matching my board (TX->PE.5 and RX->PE.4), but have been unable to communicate. I tried probing the CAN TX output from the controller and found that it is always held high irrespective of the data being sent. However on the UART (debug interface) I do not see any error messages.
Can someone please help me out with this?
Satwik