Other Parts Discussed in Thread: SW-EK-LM4F120XL
Hi
I am new to stellaris Launchpad. I wrote a program to blink LEDs and it runs perfectly on ccs debugger mode .But when i power it up separately it doesn't work .Please help me with this.
my code is
int main(void)
{
ROM_FPUEnable();
ROM_FPUStackingEnable();
ROM_SysCtlClockSet(SYSCTL_SYSDIV_5 | SYSCTL_USE_PLL | SYSCTL_XTAL_16MHZ |
SYSCTL_OSC_MAIN);
/************************************************************************************************/
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
GPIOPinTypeGPIOOutput(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3);
while(1)
{
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 4);
SysCtlDelay(4000000);
GPIOPinWrite(GPIO_PORTF_BASE, GPIO_PIN_1|GPIO_PIN_2|GPIO_PIN_3, 8);
SysCtlDelay(4000000);
}
}