I have been using the Insta-Spin GUI and am doing a project that utilizes the onboard ADC to calculate values that will then cause the motor to spin, but using the encoders, the microcontroller will know where the position of the motor is at all times. I have a question on how i can take this ADC output value, I'm assuming is in hex from the ADC example, and convert it to an RPM. However, the encoder will limit the number of rotations that the motor can do. I was wondering if anyone had any input on the structure we should be planning for this project. We have already been working tirelessly on this project, but any input and help would be very appreciated at this time.
Thanks,
Marcos.