Other Parts Discussed in Thread: RM48L950
Hello,
Please we are in desperate need for a hint!
We have "killed" 3 boards with RM48L950/952 by accident.
Two of them (1 was a Hercules HDK-card), we dont know what has happend, suddenly we cannot make our IAR debugger work with the cards!
Now we have just "killed" a card more, after we have programmed it to run with an external-2 clock of 32kHz.
Now I have changed the configuration back to run with oscillator of 20MHz, but when I try to download the program in the MCU, the debugger says it cannot get status from the MCU and the debug-session is terminated.
I have tried to get the JTag interface to connect to the MCU and get the MCU ID. This works!!!
My question is: Is it possible to get the MCU in a deadlock where the JTag works but it cannot flash the code into it?
If your answer is yes, my next question is of course, how do I get it out of this?
Best regards
Michael c".)