Other Parts Discussed in Thread: LM3S811
I just got the letter about the TIVA parts. It looks to me like the M4 parts were renamed, but that is about it. I am very disappointed for several reasons:
1. There seems to be no plans to handle M3 parts in a reasonable fashion. I have seen many posts complaining about the drop the M3 strategy, with no replacements. I have noticed it has gotten harder to get the documents for the M3 chips. I have also noticed the TI E2E forums turning into a place where engineers are recommending competition chips to replace those M3 parts that people were using! That was actually kind of funny!
2. For engineers like me who have been using TI parts for well over 30 years the biggest hit was that TI has made no effort to fill in the new TIVA or M4 lines with components over the whole product spectrum. I was using low end, low pin count parts to handle some mundane, but necessary tasks. With the new line the smallest package size is 64 pins, when I could actually do with a dual UART chips with 14 pins if it were available. Not everyone needs every interface.
3. I find it amazing to see that with each new version of the chips that TI is keeping the performance limited to 80 Mhz max. That may have been good 3 years ago, but it is not a good omen for most of us. We usually try to do more, in less time, in less space, and these new designs look more like anchors when the competition is continually improving performance with each new model.
I would like to get this to someone at TI who actually makes some decisions about what is coming up next in the TIVA world. At this point I am pretty disgusted with TI's lack of leadership in a market they are capable of dominating with a few logical product placement decisions. I would like to see a more complete top to bottom offering of choices in peripherals, with top speeds in the 150 - 250 Mhz range, in packages from 24 pin to whatever you think you need for every peripheral known to man.
Sincerely,
Mike Fontes