This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SD card Spi interface

Hi, I'm working with SD card memory device and this week I received suggestion to use SD-card example of board ek-lm4f232 on stellaris Launchpad. After check this code I identify that file: mmc-ek-lm4f232h5qd.c has all definition to connect hardware and firmware ( Is this information is True?). After check code I see that prpbabily is necessary change spi funcions to file system FATFS work well: 

For example: On spi master code of Launchpad stellaris were, the code use: 

SSIDataGet(SSI0_BASE, &ulDataRx[ulindex]); and SSIDataPut(SSI0_BASE, ulDataTx[ulindex]); and EK-lm4f232 use 

ROM_SSIDataPut(SDC_SSI_BASE, 0xFF); /* write dummy data */

ROM_SSIDataGet(SDC_SSI_BASE, &rcvdat); /* read data frm rx fifo */ 

I need change functions? 

Thanks too much