Hi
I want to interface SSI/SPI with External MAX7456 over LM4F232H5QD EVM as master SSI1
I try to Init the SSI1 as Master For example like the SSIInit() function...
And Set SSITransfer() to write and read data from the chip by SSI1 protocol.
I use for example SSITransfer(0x81, 1, pucCmd, 1); to read register 0x81 but I did not get data from the chip Why?
void SSIInit(void)
{
unsigned long ulIdx;
unsigned long ulDataTx[NUM_SSI_DATA];
unsigned long ulDataRx[NUM_SSI_DATA];
unsigned long ulindex;
//
// Enable the peripherals used by this example.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
//
// Enable processor interrupts.
//
IntMasterEnable();
//
// Configure the appropriate pins to be SSI instead of GPIO. Note that
// the chip select is kept as a GPIO to guarantee the appropriate
// signalling to the Atmel device.
//
GPIOPinTypeGPIOOutput(GPIO_PORTD_BASE, SSI_CS);
GPIOPinWrite(GPIO_PORTD_BASE, SSI_CS, SSI_CS);
GPIOPinTypeSSI(GPIO_PORTD_BASE, SSI_CLK | SSI_TX | SSI_RX);
// Enable port PD3 for SSI1 SSI1TX
GPIOPinConfigure(GPIO_PD3_SSI1TX);
// Enable port PD1 for SSI1 SSI1FSS
GPIOPinConfigure(GPIO_PD1_SSI1FSS);
// Enable port PD0 for SSI1 SSI1CLK
GPIOPinConfigure(GPIO_PD0_SSI1CLK);
// Enable port PD2 for SSI1 SSI1RX
GPIOPinConfigure(GPIO_PD2_SSI1RX);
//
// Configure the GPIO settings for the SSI pins. This function also gives
// control of these pins to the SSI hardware. Consult the data sheet to
// see which functions are allocated per pin.
// The pins are assigned as follows:
// PD3 - SSI0Tx
// PD2 - SSI0Rx
// PD1 - SSI0Fss
// PD0 - SSI0CLK
//
GPIOPinTypeSSI(GPIO_PORTD_BASE, GPIO_PIN_3 | GPIO_PIN_2 | GPIO_PIN_1 | GPIO_PIN_0);
//
// Configure and enable the SSI port for SPI master mode. Use SSI0,
// system clock supply, idle clock level low and active low clock in
// freescale SPI mode, master mode, 1MHz SSI frequency, and 8-bit data.
// For SPI mode, you can set the polarity of the SSI clock when the SSI
// unit is idle. You can also configure what clock edge you want to
// capture data on. Please reference the datasheet for more information on
// the different SPI modes.
//
SSIConfigSetExpClk(SSI1_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_3, SSI_MODE_MASTER, 1000000, 8);
SSIEnable(SSI1_BASE);
//
// Reset the PDC SSI state machine. The chip select needs to be held low
// for 100ns; the procedure call overhead more than accounts for this time.
//
GPIOPinWrite(GPIO_PORTD_BASE, SSI_CS, 0);
GPIOPinWrite(GPIO_PORTD_BASE, SSI_CS, SSI_CS);
//
// Read any residual data from the SSI port. This makes sure the receive
// FIFOs are empty, so we don't read any unwanted junk. This is done here
// because the SPI SSI mode is full-duplex, which allows you to send and
// receive at the same time. The SSIDataGetNonBlocking function returns
// "true" when data was returned, and "false" when no data was returned.
// The "non-blocking" function checks if there is any data in the receive
// FIFO and does not "hang" if there isn't.
//
while(SSIDataGetNonBlocking(SSI1_BASE, &ulDataRx[0]))
{
}
//
// Enable the SSI interrupt.
//
IntEnable(INT_SSI1);
}
//*****************************************************************************
//
// This will start an interrupt driven transfer to the SSI peripheral.
//
//*****************************************************************************
void
SSITransfer(unsigned char *pucDataOut, unsigned long ulOutCount,
unsigned char *pucDataIn, unsigned long ulInCount)
{
//
// Save the output data buffer.
//
g_pucDataOut = pucDataOut;
g_ulOutCount = ulOutCount;
//
// Save the input data buffer.
//
g_pucDataIn = pucDataIn;
g_ulInCount = ulInCount;
//
// Compute the number of extra bytes to send or receive. These counts make
// the number of bytes transmitted equal to the number of bytes received;
// a requirement of the SSI peripheral.
//
if(ulInCount > ulOutCount)
{
g_ulOutExtra = ulInCount - ulOutCount;
g_ulInExtra = 0;
}
else
{
g_ulOutExtra = 0;
g_ulInExtra = ulOutCount - ulInCount;
}
//
// Assert the SSI chip select.
//
GPIOPinWrite(GPIO_PORTD_BASE, SSI_CS, 0);
//
// Enable the transmit and receive interrupts. This will start the actual
// transfer.
//
SSIIntEnable(SSI1_BASE, SSI_TXFF | SSI_RXFF | SSI_RXTO);
//
// Wait until the SSI chip select deasserts, indicating the end of the
// transfer.
//
while(!(GPIOPinRead(GPIO_PORTD_BASE, SSI_CS) & SSI_CS))
{
}
}