This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CAN data receive problem

Hello everyone,

I am using 2 LM4F232 Stellariswares to simulate a CAN-network.
One board sends the data while the other receives it. The sending proces is ok but I have trouble receiving the data with the other controller.
I think there's a problem with the CAN-object of the received data.

The code is on the next post,


Thanks in advance

  • #include <string.h>
    #include "inc/hw_memmap.h"
    #include "inc/hw_types.h"
    #include "inc/hw_can.h"
    #include "inc/hw_ints.h"
    #include "driverlib/can.h"
    #include "driverlib/interrupt.h"
    #include "driverlib/sysctl.h"
    #include "driverlib/gpio.h"
    #include "utils/uartstdio.h"
    #include "candata.h"
    #include "datastore.h"
    #include "usbstick.h"
    #define AANTAL 28
    //***************************************************************************************
    // Holds global flags for the start of the writing.
    //***************************************************************************************
    static unsigned long g_ulArray[AANTAL];
    //***************************************************************************************
    // Flags for the CAN bus.
    //***************************************************************************************
    volatile unsigned long g_ulMsgCount = 0;
    //***************************************************************************************
    // Initializes the CAN peripheral for receiving.
    //***************************************************************************************
    void CANDataInit(void)
    {
    tCANMsgObject rCANMessage;
    //Configure CAN0 Pins. CAN0RX -> PB4 CAN0TX -> PB5
    SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
    GPIOPinConfigure(GPIO_PB4_CAN0RX);
    GPIOPinConfigure(GPIO_PB5_CAN0TX);
    GPIOPinTypeCAN(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5);
    SysCtlPeripheralEnable(SYSCTL_PERIPH_CAN0);
    // Enable all CAN functionability.
    CANInit(CAN0_BASE);
    CANBitRateSet(CAN0_BASE, SysCtlClockGet(), 500000);
    CANIntEnable(CAN0_BASE, CAN_INT_MASTER | CAN_INT_ERROR | CAN_INT_STATUS);
    IntEnable(INT_CAN0);
    IntMasterEnable();
    CANEnable(CAN0_BASE);
    // Set the different Objects which can be recieved.
    // Initialize the message object from controllers.
    rCANMessage.ulMsgID = 0x750; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 1, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object can sync.
    rCANMessage.ulMsgID = 0x730; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 2, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object BMS read.
    rCANMessage.ulMsgID = 0x710; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 3, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object torque feedback.
    rCANMessage.ulMsgID = 0x600; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 4, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object battery state.
    rCANMessage.ulMsgID = 0x540; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 5, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object brake pedal.
    rCANMessage.ulMsgID = 0x530; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 6, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object vertical acceleration.
    rCANMessage.ulMsgID = 0x520; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 7, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object force in suspension.
    rCANMessage.ulMsgID = 0x510; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 8, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object speed / tire.
    rCANMessage.ulMsgID = 0x500; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 9, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object temperature engines.
    rCANMessage.ulMsgID = 0x490; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 10, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object temperature cooling.
    rCANMessage.ulMsgID = 0x480; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 11, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object temperature brakes.
    rCANMessage.ulMsgID = 0x470; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 12, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object temperature tires.
    rCANMessage.ulMsgID = 0x460; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 13, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object suspension travel.
    rCANMessage.ulMsgID = 0x450; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 14, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object GPS parameters.
    rCANMessage.ulMsgID = 0x440; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 15, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object steering position.
    rCANMessage.ulMsgID = 0x430; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 16, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object engine revs.
    rCANMessage.ulMsgID = 0x420; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 17, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object pedal position.
    rCANMessage.ulMsgID = 0x410; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 18, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object accelerometer x.
    rCANMessage.ulMsgID = 0x320; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 19, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object accelerometer y.
    rCANMessage.ulMsgID = 0x310; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 20, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object accelerometer z.
    rCANMessage.ulMsgID = 0x300; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 21, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object position torque.
    rCANMessage.ulMsgID = 0x100; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 22, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object datapoint error.
    rCANMessage.ulMsgID = 0x090; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 23, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object controller error.
    rCANMessage.ulMsgID = 0x080; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 24, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object dash error.
    rCANMessage.ulMsgID = 0x070; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 25, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object fatal error.
    rCANMessage.ulMsgID = 0x060; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 26, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object torque error.
    rCANMessage.ulMsgID = 0x050; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 27, &rCANMessage, MSG_OBJ_TYPE_RX);
    // Initialize the message object BMS error.
    rCANMessage.ulMsgID = 0x040; // CAN msg ID - 0 for any
    rCANMessage.ulMsgIDMask = 0; // mask is 0 for any ID
    rCANMessage.ulFlags = MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER; // enable interrupts MSG_OBJ_RX_INT_ENABLE | MSG_OBJ_USE_ID_FILTER
    rCANMessage.ulMsgLen = 8;
    CANMessageSet(CAN0_BASE, 28, &rCANMessage, MSG_OBJ_TYPE_RX);
    }
    //***************************************************************************************
    // Function that receives the data caused by the interrupt. This data will be identified
    // and added to the char array.
    //***************************************************************************************
    void CANDataReceive(int ulState)
    {
    tCANMsgObject rCANMessage;
    unsigned char rMsgData[8];
    unsigned long int ID = 0;
    // Increment the counter for messages.
    g_ulMsgCount++;
    // Reuse the same message object that was used earlier to configure the CAN for receiving messages.
    // A buffer for storing the received data must also be provided, so set the buffer pointer within the message object.
    rCANMessage.pucMsgData = rMsgData;
    // Read the message from the CAN. Message object number 1 is used (which is not the same thing as CAN ID).
    // The interrupt clearing flag is not set because this interrupt was already cleared in the interrupt handler.
    CANMessageGet(CAN0_BASE, ulState, &rCANMessage, 0);
    // Check to see if there is an indication that some messages were lost.
    if(rCANMessage.ulFlags & MSG_OBJ_DATA_LOST)
    {
    // If data loss, no message needed.
    }
    ID = rCANMessage.ulMsgID;
    UARTprintf("%s : %c : %d : %x \n", rMsgData, rMsgData, rMsgData, rMsgData); // adress of data
    UARTprintf("%s : %c : %d : %x \n", *rMsgData, *rMsgData, *rMsgData, *rMsgData); // data itself
    // Switch on the correct Object. This way we can store the data in the correct temp variabels.
    // Ignore all warnings occuring in this function. Data types are resolved in datastore.c
    switch(ID)
    {
    // ID from controllers
    case 0x750:
    {
    SetControllers(rMsgData);
    break;
    }
    // ID can sync
    case 0x730:
    {
    SetCANsync(rMsgData);
    break;
    }
    // ID bms read
    case 0x710:
    {
    SetBMSread(rMsgData);
    break;
    }
    // ID torque feedback
    case 0x600:
    {
    SetTorqueFeedback(rMsgData);
    break;
    }
    // ID battery state
    case 0x540:
    {
    SetBatteryState(rMsgData);
    break;
    }
    // ID position brake pedal
    case 0x530:
    {
    SetPoisitonBrakePedal(rMsgData);
    break;
    }
    // ID versnelling verticaal per wiel
    case 0x520:
    {
    SetAccelVertical(rMsgData);
    break;
    }
    // ID krachten in ophangingarmen ( met mask per wiel)
    case 0x510:
    {
    SetForceSuspension(rMsgData);
    break;
    }
    // ID snelheid wiel mask met wiel
    case 0x500:
    {
    SetSpeedTire(rMsgData);
    break;
    }
    // ID temperatuur motoren
    case 0x490:
    {
    SetTempEngines(rMsgData);
    break;
    }
    // ID temperatuur koelwater
    case 0x480:
    {
    SetTempCooling(rMsgData);
    break;
    }
    // ID brake temp
    case 0x470:
    {
    SetTempBrake(rMsgData);
    break;
    }
    // ID tire temp
    case 0x460:
    {
    SetTempTire(rMsgData);
    break;
    }
    // ID suspension travel
    case 0x450:
    {
    SetSuspensionTravel(rMsgData);
    break;
    }
    // ID gps parameters
    case 0x440:
    {
    SetGPSparameter(rMsgData);
    break;
    }
    // ID steering position
    case 0x430:
    {
    SetSteerPos(rMsgData);
    break;
    }
    // ID toerental
    case 0x420:
    {
    SetRevsEngine(rMsgData);
    break;
    }
    // ID pedal position
    case 0x410:
    {
    SetPedalPos(rMsgData);
    break;
    }
    // ID accelerometer z
    case 0x320:
    {
    SetAccelX(*rMsgData);
    break;
    }
    // ID accelerometer y
    case 0x310:
    {
    SetAccelY(rMsgData);
    break;
    }
    // ID accelerometer x
    case 0x300:
    {
    SetAccelZ(rMsgData);
    break;
    }
    // ID torque
    case 0x100:
    {
    SetTorquePos(rMsgData);
    break;
    }
    // ID meetpunt error
    case 0x090:
    {
    SetDatapointError(rMsgData);
    break;
    }
    // ID controller error
    case 0x080:
    {
    SetControlError(rMsgData);
    break;
    }
    // dash error
    case 0x070:
    {
    SetDashError(rMsgData);
    break;
    }
    // ID algemene error
    case 0x060:
    {
    SetFatalError(rMsgData);
    break;
    }
    // torque error
    case 0x050:
    {
    SetTorqueError(rMsgData);
    break;
    }
    // ID bms error
    case 0x040:
    {
    SetBMSerror(rMsgData);
    break;
    }
    // default
    default:
    {
    break;
    }
    }
    }
    //***************************************************************************************
    // Collect the data from the temp variables. This data is used to log the current or
    // last value of the parameters.
    //***************************************************************************************
    void CANDataLog(void)
    {
    int i = 0;
    // Collect the data.
    g_ulArray[0] = GetControllers();
    g_ulArray[1] = GetCANsync();
    g_ulArray[2] = GetBMSread();
    g_ulArray[3] = GetTorqueFeedback();
    g_ulArray[4] = GetBatteryState();
    g_ulArray[5] = GetPoisitonBrakePedal();
    g_ulArray[6] = GetAccelVertical();
    g_ulArray[7] = GetForceSuspension();
    g_ulArray[8] = GetSpeedTire();
    g_ulArray[9] = GetTempEngines();
    g_ulArray[10] = GetTempCooling();
    g_ulArray[11] = GetTempBrake();
    g_ulArray[12] = GetTempTire();
    g_ulArray[13] = GetSuspensionTravel();
    g_ulArray[14] = GetGPSparameter();
    g_ulArray[15] = GetSteerPos();
    g_ulArray[16] = GetRevsEngine();
    g_ulArray[17] = GetPedalPos();
    g_ulArray[18] = GetAccelX();
    g_ulArray[19] = GetAccelY();
    g_ulArray[20] = GetAccelZ();
    g_ulArray[21] = GetTorquePos();
    g_ulArray[22] = GetDatapointError();
    g_ulArray[23] = GetControlError();
    g_ulArray[24] = GetDashError();
    g_ulArray[25] = GetFatalError();
    g_ulArray[26] = GetTorqueError();
    g_ulArray[27] = GetBMSerror();
    // Print for Debugging purposes.
    UARTprintf("Data");
    for(i = 0; i < AANTAL; i++)
    {
    UARTprintf(" : %d", g_ulArray[i]);
    }
    UARTprintf("\n");
    // Run the USB functionability to store the data in a file.
    USBStickRun(&g_ulArray);
    }