This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VBus Launchpad connection

Other Parts Discussed in Thread: EK-TM4C123GXL

Hello,

I'm going to be trying to connect my Launchpad from an external power source other than the USB port. There is an VBus socket on the bottom left of the Launchpad that can be connected with a JST connector and maybe other similar types. I plan to connect a 5V power supply which should be in the operational range of the launchpad, knowing that this same voltage is the amount it gets from the USB connection. I was wondering if anyone knew if any precautions I needed to take into consideration before hand. I plan of having my program already loaded into the MCU so it should be just a matter of plug in the VBus with a 5V source  and let the program run?

Thanks,