Hi, I am working with stellaris Lauchpad based on LM4F120H5QR ( default of launchpad) and after compeling my code I have the follow error:
**** Build of configuration Debug for project SPI_TESTE ****
C:\ti\ccsv5\utils\bin\gmake -k all
'Building target: SPI_TESTE.out'
'Invoking: ARM Linker'
"C:/ti/ccsv5/tools/compiler/tms470_4.9.5/bin/cl470" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me -g --define=TARGET_IS_BLIZZARD_RA1 --diag_warning=225 --display_error_number -z --stack_size=256 -m"SPI_TESTE.map" --heap_size=0 -i"C:/ti/ccsv5/tools/compiler/tms470_4.9.5/lib" -i"C:/ti/ccsv5/tools/compiler/tms470_4.9.5/include" --reread_libs --warn_sections --display_error_number --rom_model -o "SPI_TESTE.out" "./spi_master.obj" -l"libc.a" -l"C:\StellarisWare\driverlib\ccs-cm4f\Debug\driverlib-cm4f.lib" "../lm4f120h5qr.cmd"
<Linking>
undefined first referenced
symbol in file
--------- ----------------
CmdLineProcess ./spi_master.obj
UARTStdioInit ./spi_master.obj
UARTgets ./spi_master.obj
UARTprintf ./spi_master.obj
disk_timerproc ./spi_master.obj
f_getfree ./spi_master.obj
f_mount ./spi_master.obj
f_open ./spi_master.obj
f_opendir ./spi_master.obj
f_read ./spi_master.obj
f_readdir ./spi_master.obj
>> Compilation failure
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "SPI_TESTE.out" not built
gmake: *** [SPI_TESTE.out] Error 1
gmake: Target `all' not remade because of errors.
**** Build Finished ****
Does anyone has an ideia of why this error is appearing? My code is attached. Thanks