This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

inline c functions

Other Parts Discussed in Thread: RM48L952

Hello all,

Just wondering if it is possible to inline C functions (and if yes how). The "inline" seems to be ignored, but perhaps I do it not the correct way.

I also tried to activate "inline functions called once" in the project options.

To check if a function is inlined I do:Debug project on target, view disassembly and check  if there is a BL instruction.

Target: RM48L952, tested with compiler 5.0.1

Thank you and best Regards!

Roger