Hi, guys!
Is there any way to program two evaluation boards on one computer with the LM Flash utility?
I have EK-LM4F232 and EK-LM3748. Even though I'm selecting the proper board from the "Configuration -> Quick Set" drop-down list, it seems that the .bin file is always flashed into the EK-LM4F232 board, no matter which one is selected.
Windows 7, 64-bit, LM FLash Build 1470